0000649743_02_en

Check External Protection

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Check that all the external protections (MCCBs, MCBs, fuses) are sized according to the specifications in the Technical Data.
Failure to follow these instructions will result in death or serious injury.
NOTE: Minimum protection ratings are specified in the Technical Data. Higher protection ratings might be required to comply with local and/or national electrical codes.

Before wiring the protective earth (PE), incoming cables and batteries it is important to ensure that all breakers used for these cables are sized correctly.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?