DOCA0084EN-13

Access to IFE Webpages

Supported Web Browsers

Browser

Version with Windows 10 and later

Microsoft Edge

81.0.416.58 and later

Mozilla Firefox

45.0 and later

Google Chrome

45.0 and later

First Access to the IFE Webpages

The IFE server name must be configured during the first access to the IFE webpages.

NOTICE
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in equipment damage.

When the IFE server is accessed for the first time with SecurityAdmin user name (Security Administrator role), the user will be asked to change the default password.

NOTE: On upgrade of IFE server before accessing the webpages for the first time, delete the browser cache.

First Access Through PC with Windows 10 and Later

Step

Action

1

Disconnect the PC from the local area network (LAN) and switch off Wi-Fi.

2

Connect an Ethernet cable from the computer to the IFE server or to the Ethernet switch inside the panel.

3

Open File Explorer.

4

Click Network and the IFE-XXYYZZ appears in the list of devices.

NOTE: If the IFE server name is not displayed in the list of devices in File Explorer, check if the PC and the IFE server are not connected through the router.

5

Double-click the selected IFE-XXYYZZ, the login page automatically opens in the browser.

NOTE: Default browser must be Microsoft Edge.

6

Enter SecurityAdmin as the user name and AAAAAAAA as the password, the home page automatically opens in the browser.

NOTE: The user name and password are case-sensitive.
NOTE: When the IFE server is accessed for the first time with SecurityAdmin user name (Security Administrator role), the user will be asked to change the default password.

7

To change the password, select My Profile from the SecurityAdmin user name arrow on the header.

The Account Details Modification page is displayed.

8

Enter Old Password, Password, Confirm Password, EmailId, and Phone to change the password.

9

Select the language from the Language box and then click Apply Changes.

10

To locate the IFE-XXYYZZ, click Device Location on the header. The ULP LED of the selected IFE-XXYYZZ blinks for 15 seconds (test mode).

11

To name the IFE-XXYYZZ, select the SETTINGS menu, go to DEVICES submenu, enter the device name and click Apply Changes.

12

Write the IFE server name on a blank device name label and stick it on the existing one.

NOTE:
  • XXYYZZ is the last 3 bytes of the MAC address in hexadecimal format.

  • Check the firewall settings if DPWS is not enabled.

Access to Webpages

Follow the Network Discovery, Name Browsing, and IP Address Browsing process to access the webpages.

The webpage access depends on the IT infrastructure.

Network Discovery

Perform the following procedure to access the IFE webpages once the IFE server name has been configured.

Step

Action

1

Connect the IFE server or the Ethernet switch inside the panel to the local area network (LAN).

2

Connect the computer to the local area network (LAN).

3

Open File Explorer.

4

Click Network, the IFE name is displayed in the list of devices.

NOTE: If the IFE server name is not displayed in the list of devices in File Explorer, check if the PC and the IFE server are not connected through the router.

5

Double-click the IFE server name which is written on the device label located on the front face of the selected IFE server, the login page automatically opens in the browser.

NOTE: Default browser must be Microsoft Edge.

Name Browsing

DNS server is mandatory.

Step

Action

1

Connect the IFE server or the Ethernet switch inside the panel to the local area network (LAN).

2

Connect the computer to the local area network (LAN).

3

Start the web browser.

4

In the address text box, enter the IFE server name which is written on the device label located on the front face of the selected IFE server.

5

Press Enter, the login page automatically opens in the browser.

NOTE: If the IFE server does not appear in the list of devices in File Explorer, check if the PC and the IFE server are not connected through the router.
NOTE: The IFE server IP address is mapped to the device label in the DNS server.

IP Address Browsing

IP static configuration has to be set.

Step

Action

1

Connect the IFE server or the Ethernet switch inside the panel to the local area network (LAN).

2

Connect the computer to the local area network (LAN).

3

Start the web browser.

4

In the address text box, enter IP address given by the IT administrator.

5

Press Enter, the login page automatically opens in the browser.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.