DOCA0084EN-13

Ethernet

Description

The ETHERNET page displays:

  • Ethernet global statistics accumulated since the IFE server was last activated.

  • Ethernet port characteristics.

The users with installer or engineer roles can make changes to the Diagnostics page settings.

Navigation to the ETHERNET Page

To view the ETHERNET page, click DIAGNOSTICS > COMMUNICATION > ETHERNET.

Ethernet Port Characteristics

Statistics

Description

ETH1 Link Speed

Operational speed (10 Mbps or 100 Mbps)

ETH1 Mode

Current mode of operation (full duplex or half duplex)

ETH2 Link Speed

Operational speed (10 Mbps or 100 Mbps)

ETH2 Mode

Current mode of operation (full duplex or half duplex)

Ethernet Global Statistics

Data

Description

Frames Received

Number of frames received

Frames Transmitted

Number of frames transmitted

Click Reset Counters to reset to 0 the statistics values.

If the IFE server is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.