DOCA0084EN-13

IFE

Description

The IFE page displays the information of the IFE server connected to the circuit breakers.

The users with Installer or Engineer roles can consult the Diagnostics pages.

Navigation to the IFE Page

To view the IFE page, click DIAGNOSTICS > IFE.

IFE Server Parameters

Parameter

Description

Serial Number

Device serial number

Commercial Reference Number

Device commercial reference number

Firmware Revision

Current firmware version

Unique Identifier

Combination of MAC address and the time

MAC Address

Unique MAC address

IPv4 Address

IPv4 address of the IFE server

IPv6 Link-local Address

IPv6 address used to communicate on the local network

Date and Time Parameters

Parameter

Description

Time Source

Source of time with which the last synchronization has happened

Last Synchronization

Elapsed time from last synchronization

NTP Synchronization Status

Status of NTP Synchronization

NTP Stratum

Describes the accuracy of NTP time. It can take values from 1 to 15 or as NA (not applicable) if NTP server is not reachable.

File System Parameters

Parameter

Description

Total Size

Total amount of the IFE server disk size in kilobytes

Used Size

Total amount of used disk size on the IFE server disk in kilobytes

Free Size

Total amount of unused disk space on the IFE server disk in kilobytes

Bad Size

Amount of corrupted disk space on the IFE server disk in kilobytes

System Parameters

Parameter

Description

CPU

Status of the CPU:

  • Nominal

  • Degraded

  • Out of service

Boot Memory

Status of the boot memory

EEPROM

Status of EEPROM

File System

Status of the file system

Ethernet PHY 1

Status of PHY 1 hardware

Ethernet PHY 2

Status of PHY 2 hardware

DDR

Status of the execution memory

IFE Server Operating Time Parameters

Statistic

Description

Operating Time

Operating time of IFE server

Device Name Configuration Procedure

Step

Action

Result

1

From the IFE menu bar, click Diagnostics.

Opens the Diagnostics page.

2

From the Diagnostics menu, in the Product Information submenu, click Device Identification.

Opens the Device Identification page.

List of Parameters in Device Identification

Parameter

Description

Device name

Device name which is updated in the device name field

Product name

Name of the product

Serial number

Device serial number

Product model number

Device model number

Firmware version

Current firmware version

Unique Identifier

Combination of MAC address and the time

MAC address

Unique MAC address

IPv4 address

IP address of the IFE server

IPv6 link local address

Address used to communicate on the local network

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.