DOCA0084EN-13

Circuit Breakers

Description

The CIRCUIT BREAKERS page allows you:

  • With any role to monitor data from the circuit breaker.

  • With Installer or Engineer role to reset minimum and maximum values of the energy and demand measurements.

  • With Operator role to control the circuit breaker.

Navigation to CIRCUIT BREAKERS Page

To view the CIRCUIT BREAKERS page, click MONITORING & CONTROL > CIRCUIT BREAKERS.

Page Layout

A

Circuit breaker identification data

B

Circuit breaker health status

C

Circuit breaker monitoring and control panel

D

Monitoring of measurements

Circuit Breaker Identification Data

The circuit breaker is identified by the following data:

  • Rated current

  • Protection type

  • Number of IO modules connected

  • Additional data according to the range of the circuit breaker

Circuit Breaker Health Status

The health status of a circuit breaker is indicated by one of the following icons:

Icon

Description

OK

Medium severity detected alarm that requires non-urgent action.

High severity detected alarm that requires immediate corrective action.

Circuit Breaker Monitoring and Control Panel

A

Drawout circuit breaker position in the cradle

B

Circuit breaker main contact position

C

Circuit breaker control mode and control status

D

Circuit breaker control options

Drawout Circuit Breaker Position in the Cradle

The position of the drawout circuit breaker in the cradle is indicated by the following icons:

Icon

Description

Drawout circuit breaker is in connected position.

Drawout circuit breaker is in test position.

Drawout circuit breaker is in disconnected position.

Circuit Breaker Main Contact Position

The position of the main contacts of the circuit breaker is indicated by the following icons:

Icon

Description

The main contacts of the circuit breaker are closed.

The main contacts of the circuit breaker are opened.

The main contacts of the circuit breaker are opened and the circuit breaker is tripped. The circuit breaker must be reset.

The circuit breaker position is unknown in case of contact position discrepancy.

Circuit Breaker Control Mode

The circuit breaker control mode is:

  • Remote control: The control options on the webpage can be used to control the circuit breaker remotely.

  • Local control: The control options are not available on the webpage. The circuit breaker is controlled locally through manual operation.

The circuit breaker control status is indicated by the following icons:

Icon

Description

The closing spring is charged and the circuit breaker is ready to close.

The closing spring is charged and the circuit breaker is not ready to close.

The closing spring is discharged and the circuit breaker is not ready to close.

Close inhibition indicates that the circuit breaker closing is inhibited by the EcoStruxure Power Commission software or IO modules or a remote controller through the communication network.

Circuit Breaker Control Options

When the circuit breaker is in remote control mode, the following control options are available:

Control Options

Description

Click this option to open the circuit breaker.

Click this option to close the circuit breaker. The circuit breaker will close only if it is ready to close.

Click this option to reset ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breakers.

For each control action:

  • A safety message is displayed.

    • Read the message and click I understand to confirm the action.

    • Click Cancel to cancel the action.

    • The result of the action (successful or failed) is displayed.

NOTE: The message confirms that the command is successfully sent or not. It does not confirm whether the complete action is successful.

Measurements

The list of measurements displayed depends on the type of MicroLogic control unit or trip unit of the circuit breaker.

Measurement are displayed in the following order:

  • Real time measurements with minimum and maximum values. For circuit breaker, the time stamp of the minimum and maximum values is also displayed.

  • Energy measurements

  • Demand measurements

The minimum and maximum values of the energy and the demand measurements can be reset by users with Installer or Engineer role.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.