DOCA0084EN-13

Data Publishing

Description

The DATA PUBLISHING page allows you to export the data selected on the Devices page by email or FTPS. For more information on Devices page, refer to Devices.

The users with Installer or Engineer roles can change the data publishing settings.

Navigation to the DATA PUBLISHING Page

To open the DATA PUBLISHING page, click SETTINGS > COMMUNICATION > DATA PUBLISHING.

Data Generation Setting

Setting

Description

Value

Logging Interval

Allows you to select the time interval for logging the data.

Data Publishing Settings

Setting

Description

Export Activated

Allows you to enable the export activation of data publishing (disabled by default).

Mode

Allows you to select the mode for data publishing by:

  • Email

  • FTPS

FTPS Server Address

Allows you to enter the FTPS server address.

Port

Allows you to enter the FTPS port number.

Directory

Allows you to enter the FTPS directory name.

User Name

Allows you to enter the user name.

Password

Allows you to enter the password.

Export Interval

Allows you to select the export interval time for:

  • Logging Interval

  • Hourly

  • Daily

  • Weekly

  • Monthly

Time of Day

Allows you to select the time for data export (Default time: 00:00).

Day of the Week

Allows you to select the day for weekly export of data (Default day: Sunday).

Day of the Month

Allows you to select the day for monthly export of data (Default day: 1st day of the month).

Manual Export

Click Manual Export to start an immediate data export based on the selected data publishing settings, regardless of the scheduled interval.

Test FTPS

Click Test FTPS to verify the FTPS connection. The IFE server transmits a text file to the configured FTPS server.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.