Real Time Data
Description
The
page provides:-
the basic readings of the selected devices in real time on
. -
the device summaries on
. -
the real-time trending for the selected device for the selected topics on
.
Single Device Pages
This page displays the basic readings of the selected devices on real-time basis. This includes circuit breaker health status with green, orange, and red indication, cradle status, load current, power, power factor, voltage, and so on.
The table shows the steps to monitor the real-time data of a device:
Step |
Action |
Result |
---|---|---|
1 |
From the IFE menu bar, click . |
Opens the menu. |
2 |
From the menu, in the submenu, select a device from . |
Displays the real-time data of the selected device. |
For BCPM devices, the auxiliary and branch circuit parameters can be monitored for real-time values. If you have Administrator privilege, you can modify or configure the circuit names for BCPM devices.
Summary Device Pages
The summary device table views provide summary of one or more selected devices.
Step |
Action |
Result |
---|---|---|
1 |
From the menu, in the submenu, click . |
Expands the tree for summary page selection choices. |
2 |
Select the to be viewed. |
Opens the device selection list. |
3 |
Select the devices from the , then click .NOTE: Click
to select all the
available devices. Click to clear all the selected devices.
|
Summary of the selected device appears. NOTE: Click
to navigate back to the device selection list.
|
Trending
Step |
Action |
Result |
---|---|---|
1 |
From the IFE menu bar, click . |
Opens the menu. |
2 |
From the menu, in the submenu, select . |
Expands the data tree for real-time data option selection and the time trending option selection. |
3 |
Select . |
Opens the real-time trending setup page. |
4 |
Select up to 4 devices from the list. |
Selects devices for trending. |
5 |
Select the topics from the list.NOTE: Only topics common to all selected devices are available
for trending. The maximum number of topics to trend is dependent on
the number of devices selected.The multiplication (product) of the
selected devices and the selected topics must be 8 or less.
|
Selects topics for trending. |
6 |
Click to open the display page. |
Opens the real-time trending display page. |
7 |
Set the trending parameters. |
Allows trending parameters to be set. |
Trending Parameters
Step |
Action |
Result |
---|---|---|
1 |
Select or trending.NOTE:
redraws the x-axis in the graph
after each sample, filling it with all the data collected since the
start of the trend. The updates the graph with the latest data after each sample
while the x-axis stays constant to show the overall trend time selected.
|
Selects graph mode. |
2 |
Choose a trend time from 1–15 minutes. This is the duration of the trend. NOTE: Data
samples are taken as fast as possible but may take longer depending
on the communications load on the Modbus-SL port.
|
Selects the amount of time of the trend. |
3 |
Select to start the trending of the selected device topics.NOTE: Trending may be stopped
before reaching the trend time by clicking
. If is pressed after stopping
the sampling, a new trend is started.
|
Starts trending. |
4 |
Press to view a log of all the sampled topics recorded during the trend time. |
Displays a log of all topic values sampled during the trend. |
5 |
Press to reselect the devices and topics to trend. |
Navigates back to the real-time trending setup page. |