DOCA0084EN-12

Modbus Serial Line

Modbus Serial Line Settings

Parameter

Settings

Baud Rate

  • 9600 bps

  • 19200 bps (Factory setting)

  • 38400 bps

Parity

  • Even (Factory setting)

  • Odd

  • None

Nb bits of Stop

  • Auto (Factory setting)

  • 1 bit

  • 2 bits

Serial line termination

  • Enabled (Factory setting)

  • Disabled

Modbus SL timeout

  • 1 s (Factory setting)

  • 0.1–0.5 s

  • 1–10 s

NOTE: When Nb bits of Stop parameter is set to Auto, the actual value is based on the parity chosen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?