DOCA0084EN-13

Preferences

Description

The PREFERENCES page allows you to set the IFE server preferences for data refreshment rate.

The users with installer or engineer roles can change the preferences settings.

Navigation to the PREFERENCES Page

To view the PREFERENCES page, click SETTINGS > GENERAL > PREFERENCES.

Preferences Settings

Parameter

Description

Value

Real Time Sample Rate

Sets how often data is read from the device in the standard monitoring table views.

Setting range: 5–60 s

Default setting: 5 s

Communications Check Rate

Sets how often a communications check is performed while the browser is displaying real-time readings in the standard monitoring table views. This function attempts to bring any out-of-service devices back into service automatically.

Setting range: 5–30 min

Default setting: 15 min

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.