DOCA0084EN-12

User Interface Layout

Overview

This graphic shows the IFE webpage user interface layout.

A

Banner

B

Menu tabs

C

Subtabs

D

Action fields

E

Display zone

Banner

The banner displays the following information at the top of all the pages.

Generic Information

Description

Date and time

Current date in the yyyy-mm-dd format.

Current time in the hh-mm-sec format.

User name checked

Name of the logged in user.

Logout

To log out the IFE webpage session, click Logout or close your browser. It is recommended to log out from the IFE webpage session when it is not in use.

Main Tabs

The main tabs are:

  • Monitoring

  • Control

  • Diagnostics

  • Maintenance

  • Configuration & Settings

Subtabs

The subtabs display the submenus under the selected main tab.

Action Fields

The action fields correspond to the selected tab and it varies.

The following table describes the action fields on user interface layout:

Action Fields

Action

Apply

Applies the changes.

Cancel

Cancels the modifications to return to the last saved settings.

Display Zone

The display zone shows the selected subtab in detail with all the related fields.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?