Modbus TCP/IP Filtering
Description
The page allows you to define the level of access for Modbus TCP/IP clients connected to IFE server.
Block Connections
You can select the maximum number of IP connections allowed, 8 or 16. Each connection can have 12 concurrent transactions simultaneously.
Max Connection
is changed. Restart the Device to Take Effect message displays
and prompts to restart the device.
If IP Filtering is enabled, you must configure the IP address of the PC in the list of allowed addresses with read/write permission for using the EcoStruxure Power Commission software.
IP Filtering
|
Parameter |
Description |
Setting |
|---|---|---|
|
|
Activates the IP address filtering. The list of IP addresses available in the table is granted access. |
|
|
|
Filters the required IP address entered by you. |
10 addresses (Maximum allowed IP addresses) |
|
|
Defines the access level for the corresponding IP address. |
|
|
|
Allows all Modbus TCP/IP clients to have the read-only access. |
|