Webpage Description
Monitoring Webpage
|
Monitoring Submenu |
Webpage |
Description |
|---|---|---|
|
|
The single device pages provide basic readings of the selected devices. |
|
|
The summary device pages provide summaries of one or more selected devices. |
||
|
The trending page view provides real-time graphic and table trending of common topics across multiple devices. |
||
|
|
The single device pages provide the graphic and table trending logs of user-selectable quantities for selected devices. |
|
|
The summary device pages provide graphic trending logs of multiple devices with a common topic. |
Control Webpage
Diagnostics Webpage
|
Diagnostics Submenu |
Webpage |
Description |
|---|---|---|
|
|
Displays diagnostic data used to troubleshoot the network-related problems. |
|
|
|
|
|
|
Displays the list of the IMU devices connected to the ULP port. |
||
|
|
Displays register data connected locally to the IFE server. |
|
|
Verifies the communications health of all the server devices connected to IFE server. |
||
|
|
Displays the status of IO module of the selected device. Displays if the selected device is not connected to a IO module. NOTE: refers to the server device name
defined in the page.
|
Maintenance Webpage
Configuration & Settings Webpage
|
Configuration & Settings Submenu |
Webpage |
Description |
|---|---|---|
|
|
|
|
|
Sets the date and time manually or sets the IFE server time automatically using an SNTP source or configures the server device connected to IFE server to synchronize their time with the IFE server time automatically. |
||
|
Configures the time zone for the region and sets the daylight saving time. |
||
|
|
Configures the Ethernet. |
|
|
Configures the IP parameters. |
||
|
Configures the maximum number of Modbus TCP/IP server connections. Configures the IP addresses that can access the IFE server through Modbus TCP/IP. |
||
|
Configures serial communication parameters. |
||
|
|
Configures the alarms to be emailed. Configures the SMTP parameter for mailing purpose. |
|
|
Configures the alarms to be sent through email. |
||
|
|
Configures local serial devices on the Modbus serial daisy chain and IMU core product connected to the ULP port of the IFE server. |
|
|
Configures device logging parameters. |
||
|
Configures device logging export options. |
||
|
|
Configures Simple Network Management Protocol (SNMP). |
|
|
Configures IFE server preferences. |
||
|
Configures the advanced service control parameters. |
||
|
Creates and edits groups and users. Configures email accounts. |
||
|
Configures webpage access rights for each user group. |