DOCA0084EN-13

Time Zone

Description

The TIME ZONE page allows you to set the time zone of a particular region.

The users with Installer or Engineer roles can change the time zone settings.

Navigation to the Time Zone Page

To view the TIME ZONE page, click SETTINGS > GENERAL > TIME ZONE.

Real Time Clock

The IFE server has a Real Time Clock (RTC) to maintain date and time during power outage. The expected life time of the RTC is 15 years when operated at intermediate mode (in this mode, the battery is operated continuously for 4 days with an interval of 45 times over a period of 10 years).

The IFE server must maintain a crystal tolerance of ±20 ppm (typical)/±150 ppm (maximum) during the period of 15 years at -25 °C (-13 °F) to 85 °C (185 °F). The time drift by RTC chip varies from -16 s/day to +2 s/day. During power recycle, the RTC is able to maintain the date and time settings.

Time Zone Settings

Parameter

Description

Time Zone Offset

Allows you to select the time zone of a particular region.

Enable

Enables the daylight saving time.

Daylight Savings Time begins

Allows you to set the start time of daylight saving.

Daylight Savings Time ends

Allows you to set the end time of daylight saving.

NOTE: The settings of Time Zone is applicable only when DATE & TIME is in Network Synchronization via NTP mode.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.