DOCA0084EN-13

Devices

Description

The following devices can be connected under IFE server. However, the Device webpage only displays the connected devices.

  • BCM ULP module

  • MicroLogic trip unit or control unit

  • BSCM module

  • BSCM Modbus SL/ULP module

  • FDM121 display

  • USB maintenance interface or UTA module

NOTE: The webpages are supported only for the devices added in the device list.

Navigation to the Devices Page

To view the DEVICES page, click DIAGONASTICS > DEVICES.

Circuit Breakers Parameters

Parameter

Description

Rated Current

Displays the rated current of the circuit breaker.

Protection Type

Displays the protection type of the circuit breaker.

Remaining service life indicator

Display the service life of the circuit breaker.

Contact wear indicators

Display the contact wear counters of the circuit breaker.

Indication contacts (OF) operation since last reset

Display the indication of contact operation of circuit breaker since last reset.

Fault trip indication contact (SDE) operation

Display the indication of fault trip contact operation of circuit breaker.

Cradle connected

Display the status of cradle in connected position.

Cradle disconnected

Display the status of cradle in disconnected position.

Cradle test

Display the status of cradle in test position.

Components Parameters

Device

Parameters

Description

Circuit Breaker

Product Range

Name of the device type.

Product Model

Device model number.

Serial Number

Device serial Number.

Commercial Reference Number

Device commercial reference number.

Firmware Revision

Current firmware version.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.