DOCA0084EN-13

Modbus Serial Configuration

Description

The MODBUS SERIAL CONFIGURATION page allows you to modify Modbus serial communication parameters.

Navigation to the MODBUS SERIAL CONFIGURATION Page

To view the MODBUS SERIAL CONFIGURATION page, click SETTINGS > COMMUNICATION > MODBUS SERIAL CONFIGURATION.

Modbus Serial Line Settings

Parameter

Settings

Baud Rate

  • 9600 bps

  • 19200 bps (Factory setting)

  • 38400 bps

Parity

  • Even (Factory setting)

  • Odd

  • None

Nb bits of Stop

  • Auto (Factory setting)

  • 1 bit

  • 2 bits

Serial line termination

  • Enabled (Factory setting)

  • Disabled

Modbus SL timeout

  • 1 s (Factory setting)

  • 0.1–0.5 s

  • 1–10 s

NOTE: When Nb bits of Stop parameter is set to Auto, the actual value is based on the parity chosen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.