DOCA0084EN-13

Set Device Time

Description

The SET DEVICE TIME page allows you to synchronize the date and time of the IMU devices connected to the IFE server to IFE server date and time. It also allows you to get the device time and set device time that are connected to the IFE server. This page lists the IMU devices that are stacked to the IFE server to set their date and time.

List of Parameters in Set Device Time

Parameter

Description

Device Selection

Allows you to select the device from the list for synchronizing, getting, and synchronizing the time.

Localized Time

Displays the time of the selected device.

Status

Displays the status of the selected device.

Get Time

Allows you to get the time of the selected device.

Set Device Time

Allows you to set the time of the selected device.

Setting the Device Time

Step

Action

Table

1

From the IFE menu bar, click Settings.

Opens the Settings menu.

2

From the Settings menu go to General and click Set Device Time.

Opens the Set Device Time page.

3

Select the devices from the Set Device Time page, and then click Set Device Time.

The selected server device date and time gets synchronized with the IFE server time and the status is updated as successful.

NOTE: If the selected device fails to synchronize with IFE server date and time, then the status is updated as unsuccessful.
NOTE: Set Device Time feature is not applicable for IFE server’s own IMU and shows the set status as NA (Not Applicable).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.