DOCA0084EN-10

Device Log Export

Description

The Device Log Export page is used to export the device logs automatically by IFE server. The device log export allows you to configure IFE server to export device logs periodically. You can choose to export the device log files through email or FTP.

NOTE: If the email and the FTP servers are not located on the same Ethernet network segment as the IFE server, ensure that the IFE default gateway is properly configured.

Transport

Parameter

Description

Setting

Disabled

When Disabled is selected, either email or FTP is enabled.

Email

Allows you to choose the way of exporting the log files through email.

FTP

Allows you to choose the way of exporting the log files through FTP.

NOTE: When FTP is selected, Test FTP is enabled.

Test FTP

Sends the text file to the FTP server configured in the FTP parameters. The text file contains the device information, and the device name with the date and time.

Incremental

Selects only the new interval data logged since the last successful data export.

NOTE:
  • If the transport is scheduled for Hourly or Logging Interval, the incremental check box is selected automatically and is unavailable to be cleared.

  • If the Incremental check box is not selected, the complete log file is sent through an email as an attachment on each scheduled interval.

Manual Export

Allows you to export the accumulated log files manually.

Schedule

Parameter

Description

Setting

Logging Interval

Selects how often the data logs are sent.

  • Hourly

  • Daily

  • Weekly

  • Monthly

  • Logging Interval

To Addresses

Parameter

Description

Setting

To Addresses

Lists the email recipients configured in the IFE user accounts.

FTP Parameters

Parameter

Description

Setting

Server IP Addresses

Allows you to enter the FTP server IP address.

Server TCP Port

Allows you to enter the server port number.

Directory

Allows you to select the directory where you want the files to be saved.

Username

Allows you to enter the FTP username.

Password

Allows you to enter the FTP password.

Passive

Allows you to select the mode of FTP operation.

NOTE: Passive mode is enabled by default.

QR code for this page

Was this helpful?