Schematics with MasterPacT MTZ Circuit Breakers
Description
The IFE server is connected to the MasterPacT MTZ circuit breaker with MicroLogic X control unit through its ULP port module.
For more information on the ULP System and its components, refer to the ULP System User Guides in Related Documents.
ULP Connection
NOTICE |
---|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All the connection configurations require the RJ45 plug/plug ULP cord.
When the second RJ45 ULP port is not used, it must be closed with an ULP line termination.

A |
RJ45 plug/plug ULP cord |
B |
ULP line termination |
Connection of the IFE Server to a MasterPacT MTZ Circuit Breaker with MicroLogic X Control Unit
Connect the IFE server to the ULP port module on a MasterPacT MTZ circuit breaker with MicroLogic X control unit by using the ULP cord.

A |
IFE Ethernet switchboard server |
B |
ULP line termination |
C |
RJ45 plug/plug ULP cord |
D |
ULP port module |
E |
MasterPacT MTZ fixed circuit breaker with MicroLogic X control unit |