Restore the Smartlink Modbus Devices
Description
The IFE server to the Smartlink Modbus device. The page displays the information about the device name, device type, and device status.
submenu allows you to move the configuration settings from the-
IFE firmware versions that are less than or equal to V001.009.008.
-
Smartlink Modbus devices and the IFE firmware versions that are equal to or greater than the versions listed in the system compatibility table for Smart Panels 1.1 and later.
Restore Page Parameters
Parameter |
Description |
Settings |
---|---|---|
|
Allows you to select the desired Smartlink Modbus device to restore the configuration in the Smartlink Modbus device. |
NOTE: The check box is unavailable if the Smartlink
Modbus device is not connected or the Smartlink Modbus device has
incompatible firmware version
|
|
Displays the name of the IFE server. |
– |
|
Displays the name of the Smartlink Modbus device entered in the device list. |
– |
|
Displays the device type selected for the Smartlink Modbus device in the device list. |
– |
|
Displays the restore status of the Smartlink Modbus device. |
|
|
Allows you to restore the configuration in the Smartlink Modbus devices. |
– |
Restoring the Smartlink Modbus Device Configuration
Step |
Action |
Result |
---|---|---|
1 |
From the IFE menu bar, click . |
Opens the menu. |
2 |
From the menu, click submenu. |
Displays the page. |
3 |
From the page, select the Smartlink Modbus devices to restore the configuration. |
Selects the desired Smartlink Modbus devices to restore the configuration. |
4 |
Click . |
dialog box appears. |
5 |
Click . |
Configuration is restored in Smartlink Modbus devices from IFE server. |