TeSys™ Giga Series

Refer to Catalog MKTED210011EN

Giga Replaceable Switching Modules

LA9G3QA

  • Innovative contact switching modules for TeSys™ Giga Contactors

  • Replace worn-out poles with a new switching module in minutes, without having to disassemble the entire product.

  • No special tools are needed for the replacement

TeSys™ Giga – Switching modules for TeSys Giga contactors (Standard and Advanced versions)

Description

Suitable for:

For contactors

Reference

3 or 4 switching module kits

3-pole

LC1G115/LC1G225

LA9G3QA

LC1G265/LC1G330

LA9G3RA

LC1G400/LC1G500

LA9G3SA

LC1G630/LC1G800

LA9G3TA[1]

4-pole

LC1G115/LC1G225

LA9G4QA

LC1G265/LC1G330

LA9G4RA

LC1G400/LC1G500

LA9G4SA

LC1G630/LC1G800

LA9G4TA[1]

note

During replacement, replace all switching modules. After replacement, change the position of the RESET button on the control module from A to B or B to A.

Footnotes

  1. Available 2Q 2022.
Feedback