TeSys™ Deca Enclosed Combination Starters

Refer to Catalog MKTED210011EN

Insta-Kits Selection

From top to bottom: Start/Stop, On - Off Selector Switch, HOA Selector Switch

With the use of Insta-Kits, only one operator scheme is allowed. For additional accessory kits and options, see Catalog 8100CT1901. Check with local sales office for availability.

TeSys™ Deca AC Magnetic Starter, 2–3 Pole

Insta-Kit Accessories for Field Installation

Symbol

Description

Color

Nameplate

Suffix/Cat. No. [1]

NEMA Type 1

One operator on cover

2 Position selector switch

Black

Off - On

LA9CA06DT

3 Position selector switch

Black

Hand - Off - Auto

LA9CA06ET

2 Push buttons

Green

Red

Start

Stop

LA9CA06GT

3 Position selector switch, Pilot light (transformer type)

Black

Red/Green

Hand - Off - Auto

Power On

LA9CA06UT

Footnotes

  1. Catalog numbers beginning with LA9 are only for starters with a “2” before the voltage code. When using a factory option that does not have a corresponding customer kit, the 10th digit of the starter must change from a "2" to a "1".

Feedback