ADMS ArcFM Tools

There are two primary toolsets that facilitate the integration between ArcFM and ADMS as part of Schneider Electric ’s EcoStruxure:

  • ArcFM Redlining Tools

    • This toolset’s functionality is the same whether the redlines originate from ADMS or ArcFM Mobile.

  • ADMS QA/QC Rules

    • These tools are used only when you have ArcFM integrated with Schneider Electric ’s ADMS solution.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?