ArcFM Inset Frames

The ArcFM Inset Frames tool allows you to display specific features within your current view individually in separate windows. For example, you can depict each switching facility in the Switching Facility layer in its own inset frame. These individual inset frames are shown in a window.

Inset frames are available in both ArcFM and ArcFM Viewer. Inset Frame Source Feature Classes is available in ArcFM only.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?