Attribute Viewer
The Attribute Viewer allows you to view
the attribute fields of selected features. The ArcFM Display Field
is the value displayed on the Attribute Viewer. The default ArcFM
Display Field is the ObjectID, which administrators can change in
ArcCatalog. In the example below, the display field is the Facility
ID. Users can view relationship classes and expand related objects
that are indicated by the plus icon.
You can access ArcFM utility tools by right-clicking on features in the Attribute Viewer. Select: Zoom To, Pan To, Quick Attribute Viewer, Highlight, Remove from Selection, or Feeder Manager Translator (electric data only).
You may also access utilities tools when you right-click related objects. These tools allow you to view the Quick Attribute Viewer or remove all objects from the selection.
When using the Locator tool, you can use the Add to Selection utility in the Locator results tree to add features listed in the search results to the Attribute Viewer Selection tab.