Post Session
An Approval Officer may post a session in ArcFM . This tool is not available in ArcFM Viewer for ArcGIS Engine. You must access Session Manager through ArcMap and be logged in to SDE to post a session.
The Post Session button initiates a task also called “Post Session.” The out-of-the-box subtasks for this parent task are:
-
Close session
-
Post version
-
Delete version
-
Delete session
These subtasks can be modified by an administrator so that the Post Session parent task completes other functions as a part of your company’s workflow. See the Configuration topic Process Framework Administration Tools for more information.
To post a session in ArcFM:
- Open the session to be posted.
- Ensure you have reconciled the session first. The Post Session button is disabled until the session has been reconciled. If you are using an Access database, the Post button remains enabled and the session does not have to be reconciled.
-
Click the Post Session
button on the Session Manager toolbar.
When the Approval Officer clicks the Post Session button, the version associated with the session is posted to the parent version.