Mobile Enterprise

Mobile Enterprise encompasses the tasks performed by the enterprise editor to prepare a session or design (Designer only) for the field and utilize the edit packet upon its return from the field.

Work Flow Example 1: Sessions

Work Flow Example 2: Designs

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?