Stored Items Options

Use the Options to determine display settings for the ArcFM Stored Items list. To open the Options dialog, select Options from the Stored Items pull-down on the ArcFM toolbar.

Display: Select the checkboxes for the user interface elements you want to display in the Stored Items list. By default, all checkboxes are selected.

Settings: The Maximum size of Most Recently Used List setting determines the maximum number of items that may be displayed in the Most Recently Used list.

Auto Expand Folders: Select a radio button to indicate the number of levels to expand folders when the tab is selected.

The following image shows first level stored displays:

The following image shows the first two levels:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?