Select Parcels
The Select Parcels step has four tools you can use to select a set of parcels for your optimized layout. Designer displays the selection set graphically on the map. The nodes in the selection set are also available in the Design Optimization tree. Right-click any item to access the available context menu tools (e.g., Remove, Highlight, Zoom To).
You can remove a parcel from the selection using the tools detailed below. You may also right-click the parcel in the tree and select Remove.
Add Parcels to Selected Set
You can add one or more parcels to an existing selected set before or after optimizing:
- Use the Select Parcels tool to select the parcel that you want to add to the selected set.
-
Use Group Parcels to regroup the entire selected
set including the new parcel.
- You can now run Optimize Secondary Circuits. The optimized results account for the newly added parcel.
-
To add additional parcels AFTER optimizing, first select
the desired parcels and then use Associate Parcel to New Transformer. You can associate one parcel to a new transformer at a time.
NOTE: Additional parcels cannot be added to the selected set after running Complete All.