Submit Mobile Session or Design

After the field editor has completed a session or design in the field, it may be submitted for approval.

  1. Select the session or design to be submitted.
  2. Choose the appropriate task from the Available Tasks menu:
    • Session: Submit Mobile Session

    • Design: Submit Mobile Design

  3. Click the green arrow to execute the task.
  4. Select an Approval Officer from the list.
  5. Click OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?