Quick Estimate

Use the Quick Estimate toggle button to send compatible units (CUs) directly to the Design tab in the Attribute Editor. Use this tool to assemble a collection of CUs, then view a Design Cost Report for a cost estimate on the design.

 Click the Open Design Cost Report button to view the design costs.

Quick Estimate toggle button status:

enabled - CUs are sent to the Design tab when you double-click them or press Enter with CUs selected.

disabled - CUs are sent to Targets tab by default when you double-click them. Access the right-click menu to send CU to Design tab.

NOTE: Non-GIS CUs are always sent to the Design tab, regardless of the Quick Estimate setting. If no design is open, non-GIS CUs will not be sent to the Attribute Editor.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?