Conduit System

Configuring your conduit system allows you to define the number, size, and type of ducts available in each conduit feature. Once the ducts are defined, you can associate conductors and cables with specific ducts within the conduit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?