All Feeders, Multiple-Feed Feeders, or Feeders with Loops
All Feeders locates all devices belonging to a given feeder or set of feeders. Select Multi-Feed Feeders to find all feeders that have more than one source of electric power. Feeders with Loops locates all feeders that create electrical loops.
-
Select an Energized Phase. The value in this field allows
you to find all features associated with a feeder or group of feeders
associated with a specific phase.
NOTE: For conductors, the energized phase information within the FeederInfo field is determined using the field with the PHASEDESIGNATION field model name assigned. Therefore the energized phase matches the phase designation. For devices however, the energized phase does not match the phase designation.
- Select the Locate Lines Only (or Locate Lines with Loops Only) checkbox to view only conductor features.
- Choose a Substation.
- Select a feeder from the grid.
- Click Close.
- Press Enter or click Find in the ArcFM Locator window to perform the search. Click the Stop button if you want to end the search before it is complete.