Building an Export Set in Design Summary

The Design Summary form allows you to select the CUs you want to export. By default, all CUs are selected. You can scroll through the list to uncheck CUs to deselect them, or you can refine the list shown using the search and toggle buttons.

In Design Summary, CUs in a given work location are grouped by their Work Function, while linear features are aggregated. In addition to exporting the selected CUs in the Design Summary form, you can include notes in the Export Notes field that are also exported in the summary. Once you are ready to export the summary, you have the choice to export to HTML or Excel. For more see Design Summary Export Tools.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?