Add Circuit

Follow this procedure when adding a new circuit to your feeder system:

  1. With an editing session started, add the Circuit Source feature class (e.g., Dynamic Protective Device) to the Targets tab and expand the class.
  2. Right-click Circuit Source and select Add Related Object to create a relationship between the circuit source feature class (e.g., Dynamic Protective Device) and the CircuitSource object.
  3. Enter values in the FeederID, FeederName and SubstationID fields.

      

  4. Place the feature on the map.
  5. Continue to add features to the new source. The Feeder Manager autoupdaters will dynamically update the FeederID value for all features added to the feeder.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?