Conduit Tracing

The Conduit Manager trace task allows you to identify available ducts in your underground network. Conduit Tracing is available whether you have Conduit Manager licensed or not. Users may access Conduit Tracing tools from ArcFM and ArcFM Viewer. Also, you must select the network you created for conduit tracing in the Utility Network Analyst toolbar's Network field.

IMPORTANT: In order to perform a trace, the Enabled fields on the features in the geometric network must be set to True. Any feature with an Enabled value of False will be treated as a barrier in the trace.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?