Conduit Trace Report

Conduit Manager allows you to generate a report based on a conduit trace. To generate a report, simply select the checkbox on the Conduit Traces tab of the Options.

When you run the Conduit trace, a Conduit Trace Report will be generated and appear in a browser window. The report will list the Criteria Summary, followed by a feature list which lists junctions and edges in order of the trace, from the starting flag to the ending flag. Each feature will be followed by its attributes.

If the feature is a conduit system feature, any subducts which meet the query criteria will be listed.

Report

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?