ArcFM Viewer Options

There are several options listed in the ArcFM Viewer Options in the Customize menu.

  • The General options tab allows you to determine the Zoom To scale, the size of the flash for the Highlight tool, and other options.

  • The Attribute Viewer options tab allows you to show a status bar that indicates the number of items selected. When enabled, the status bar may be found at the bottom of the Attribute Viewer. This tab also allows you to determine the order in which features appear on the Selection tab. You may choose from drawing order or alphabetical order.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?