Stored Items List
This drop-down menu is available on the ArcFM and ArcFM Viewer toolbars and displays three tabs that allow you to open page templates, stored displays or documents. It also displays the name of the currently selected stored item (if there is one).

There are two ways to select a stored item from the Stored Items field. Type-ahead functionality in the field displays stored items as you type. The icons next to the stored item names indicate the type:
You may also select a stored item using the tabbed interface:
- Click the arrow on the drop-down menu to display the tabs.
- Select a tab.
- Double-click the stored item you want to open, or right-click it and select Open.
- After you've opened a stored item, the Most Recently Used list may be displayed on that tab (depending on the Options settings).
-
Double-click an item in the Most Recently Used list to
select it.
If the list becomes too long to view in the window, you can click and drag the edge of the drop-down window to expand it to be longer and/or wider. Use the Stored Items Manager to create, modify or delete stored items.