ArcFM Viewer Toolbar
The ArcFM Viewer toolbar provides access to a collection of tools that increases productivity and functionality in ArcMap sessions. If the ArcFM Viewer toolbar is not displayed, click View > Toolbars, then check the ArcFM Viewer toolbar on the dropdown list. Or, you can right-click in the gray toolbar area and select ArcFM Viewer from the list. This toolbar is dockable.
To add buttons to the toolbar:
- Right-click the gray area of the toolbar and select Customize.
- Select the Commands tab and click ArcFM Solution as the Category.
-
Drag icons from Commands and drop on the toolbar.
To remove buttons from the toolbar:
- Right-click the gray area of the toolbar and select Customize.
-
Drag the button from the toolbar and drop it anywhere off
the toolbar.
To restore default buttons:
- Right-click the gray area of the toolbar and select Customize.
- Click the Toolbars tab.
- Highlight ArcFM Viewer.
-
Click Reset to restore any removed default buttons.
The following buttons appear on the ArcFM Viewer toolbar by default:
The following buttons do not appear on the ArcFM Viewer toolbar by default. These may need to be added using the steps above.
The following buttons have been replaced by the Stored Items tools. These three buttons are still supported and now reside on the ArcFM Stored Items Classic toolbar.