Remove From List

This right-click utility appears on items in the Targets tab. It allows the user to remove selected items from the Targets tab.

  1. Select one or more features on the Targets tab. Use the Shift key or Ctrl key to select multiple items.
  2. Right-click and select Remove From List.

    The tool will remove the selected features or objects from the Targets tab. It does not delete or remove items from the map.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?