Attribute Query
This search method allows you to query specific attribute fields to find features.
-
Click the Locator tool
icon on the ArcFM toolbar to display the ArcFM Locator.
- Select Attribute Query from the pulldown list.
- Select the layer you want to search.
- Select the Show all tables checkbox to expand your search to include all tables in your geodatabase. If you have gas features in one dataset and electric features in another and select this box, the Locator tool will search both gas and electric features.
-
Select the Use all map sources checkbox to expand
your search further to include all tables from all databases that
are present in the map. If you have landbase features from one
database and water features from a different database in the map,
selecting this box will prompt the Locator tool to search tables
from both databases.
IMPORTANT: Searching tables from all databases could have a performance impact if you have many databases in the map at once.
- Select the Ignore Subtypes checkbox to perform your search across all subtypes of the feature class selected in the Search field.
- Type values of the attributes for which you want to search. Edited attribute field names are displayed in blue text. If a field does not accept a Null value and no value is assigned, it is highlighted in yellow.
- Click the Options button to open the Locator Options dialog. Select Auto Zoom to Results to automatically zoom in on the found set of features. If the user clicks the Stop button before the search is complete, the Auto Zoom will NOT zoom to the found set.
- In the Locator Options dialog you can also select Auto Add to Selection to automatically select the found set on the map and append it to the Selection tab of the Attribute Viewer. If the user clicks the Stop button before the search is complete, the found set will be selected. This field will be disabled if the layer you're searching is not selectable or is a table.
- When you click Find or press Enter, the Locator lists features that meet the search criteria in the window. If desired, you can use the right-click menu to add features to the Selection tab of the Attribute Editor.