Underground Facility Manager

The Underground Facility Manager (UFM) allows you to view underground structures and navigate the underground facilities network. The Underground Facility Diagrams toolbar offers navigation tools as well as buttons that allow you to select the diagram or a duct bank. Underground structure features (e.g., walls, floor, duct banks) are visible only if they have been placed on the map. These features are created using Conduit Manager in ArcFM.

ArcFM Underground Facility Diagrams Toolbar

This toolbar provides the tools to view existing underground facility diagrams. Not all tools displayed on the toolbar are available in ArcFM Viewer. The tools discussed below are available in ArcFM Viewer to allow you to view underground facilities. All other tools on this toolbar will remain disabled.

Launch Diagram Manager

Use this tool to view an existing diagram and open the Diagram Manager.

Close Diagram Manager

Click this button to dismiss the Diagram Manager window.

Navigate to Next Facility

Click this button, then click a duct bank to navigate to the next underground facility. Use this tool to navigate through the underground facilities network.

Navigate to Previous Facility

Click this button to navigate to the previous underground facility. This button will remain disabled until the Navigate to Next Facility button has been used.

Select Diagram

Click this button to select the current underground facility diagram. You may view information about the individual selected features on the Attribute Viewer.

Select Duct Bank

Click this button, then click a duct bank to select it. You may view information about the individual selected features on the Attribute Viewer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?