DOCA0106EN-15

Recover EIFE Interface from Boot Mode

During a firmware upgrade, if any communication disturbance occurs and files are not transferred successfully, the EIFE interface can transition to boot mode.
  1. Connect EIFE interface to a circuit breaker using a ULP cable.
  2. Change the IP address of connected PC to 169.254.XX.XX. You can enter any value between 1 to 254 for XX.XX.
    NOTE: You can refer to Microsoft Windows Help for performing step 2 and 3.
  3. Set the subnet mask to 255.255.0.0.
    NOTE: This ensures the PC is configured within the same IP address range of the EIFE interface in boot mode.
  4. Open the EcoStruxure Power Commission software.
  5. Sign in to EcoStruxure Power Commission software.
  6. Discover the EIFE interface, which is in the boot mode.
    NOTE: The current firmware version of EIFE interface is displayed as EIFEBOOT.
  7. Initiate the firmware update process.
    After the firmware update, the EIFE interface reverts to its original IP address.
  8. Restore the PC network settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.