Status
Description
The page displays the EIFE interface communication status.
While browsing the real-time data views, the EIFE interface has an automated communication check that runs every 15 minutes by default. This check verifies the communication health of all the devices configured on the EIFE interface, and attempts to re-establish the communication to any device marked out of service within the current browser session.
A manual communication check is possible by clicking .
The users with installer or engineer roles can change the Diagnostics page settings.
Navigation to the Status Page
To view the page, click .
Status Parameters
|
Data |
Description |
|---|---|
|
|
Name of the device connected to EIFE interface. |
|
|
Type of the device connected to EIFE interface. |
|
|
Displays the connection type: Type 1: ULP |
|
|
Status of communication:
|