990-91430E-037

通信接口概述

  1. TCP/IP

  2. 干接点端口

  3. SMPS I/O

  4. CAN I/O

  5. RS485

  6. 系统 BMS CAN I/O

  7. DC OUT 1、DC OUT 2

  8. 重置开关

  9. 开机按钮

  10. DC IN 1、DC IN 2

  11. 状态指示灯

  12. CAN 总线回路端接电阻开关

  13. 端口 CAN 1、CAN 2

  14. 模块

  15. EPO

  16. PSU 1 LED

  17. PSU 2 LED

  18. SG IO 1

  19. SG IO 2

  20. MCCB AUX 1

  21. MCCB AUX 2

反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.