DOCA0084EN-10

Schematics with MasterPact NT/NW and ComPact NS Circuit Breakers

Description

FYI, this map is shared by IFE user guide and NT/NW Modbus guide.

Depending on the type of circuit breaker used, connect the IFE server to the circuit breaker using one of the following configurations:

  • Connection of the IFE server to a fixed manually-operated ComPact NS circuit breaker with a BCM ULP module.

  • Connection of the IFE server to a fixed electrically-operated MasterPact NT/NW or ComPact NS 630b-1600 circuit breaker with a BCM ULP module.

  • Connection of the IFE server to a drawout MasterPact NT/NW or ComPact NS 630b-1600 circuit breaker with a BCM ULP module and its respective IO module.

For more information, refer to the ULP System User Guide.

ULP Connection

NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Never connect an Ethernet device to a RJ45 ULP port.
  • The RJ45 ULP ports of IFE server are for ULP modules only.
  • Any other use can damage the IFE server or the device connected to the IFE server.
  • To check if a ULP module is compatible with the RJ45 ULP ports of IFE server, refer to the ULP System User Guide.
Failure to follow these instructions can result in equipment damage.

All connection configurations require the BCM ULP cord.

When the second RJ45 ULP port is not used, it must be closed with a ULP line termination.

A

Circuit breaker BCM ULP cord or RJ45 male/male ULP cord

B

ULP line termination

Connection of the IFE Server to a Fixed Manually-Operated ComPact NS Circuit Breaker

A

IFE Ethernet switchboard server

B

ULP line termination

C

Circuit breaker BCM ULP cord

D

BCM ULP circuit breaker communication module

E

Fixed manually-operated ComPact NS circuit breaker

Connection of the IFE Server to a Fixed Electrically-Operated MasterPact NT/NW or ComPact NS 630b-1600 Circuit Breaker

A

IFE Ethernet switchboard server

B

ULP line termination

C

Circuit breaker BCM ULP cord

D

Fixed terminal block

E

BCM ULP circuit breaker communication module

F

Fixed electrically-operated circuit breaker

Connection of the IFE Server to a Drawout MasterPact NT/NW or ComPact NS 630b-1600 Circuit Breaker

A

IFE Ethernet switchboard server

B

ULP line termination

C

RJ45 male/male ULP cord

D

Circuit breaker BCM ULP cord

E

Circuit breaker disconnected position contact (CD)

F

Circuit breaker cradle

G

BCM ULP circuit breaker communication module

H

Drawout circuit breaker

I

Drawout terminal block

J

Circuit breaker connected position contact (CE)

K

Circuit breaker test position contact (CT)

L

IO input/output application module for one circuit breaker

QR code for this page

Was this helpful?