IO Readings
Description
The IO module input/output configuration. It displays six digital inputs, three digital outputs, and one analog input. The IO application control is possible only when the IO module is connected to a circuit breaker.
page shows theThe table shows the steps to access the
page:
Step |
Action |
Result |
---|---|---|
1 |
From the IFE menu bar, click . |
Opens the page. |
2 |
From the menu, select a device from submenu. |
Opens the page for the selected device. |
List of Parameters in IO Module
Parameter |
Description |
Setting |
---|---|---|
|
Displays the six digital inputs configured in the IO module. |
– |
|
Displays the three digital outputs configured in the IO module. |
– |
|
Displays the analog input assigned in the IO module. |
– |
|
Displays the assigned functions of the corresponding inputs or outputs. |
– |
|
Displays the value of the six digital inputs and three digital outputs |
|
|
Displays the six digital inputs and three digital outputs are forced or unforced |
|