IFE
Description
The IFE page displays the information of the IFE server connected to the circuit breakers.
The users with Installer or Engineer roles can consult the Diagnostics pages.
Navigation to the IFE Page
To view the IFE page, click .
IFE Server Parameters
Parameter |
Description |
---|---|
|
Device serial number |
|
Device commercial reference number |
|
Current firmware version |
|
Combination of MAC address and the time |
|
Unique MAC address |
|
IPv4 address of the IFE server |
|
IPv6 address used to communicate on the local network |
Date and Time Parameters
Parameter |
Description |
---|---|
|
Source of time with which the last synchronization has happened |
|
Elapsed time from last synchronization |
|
Status of NTP Synchronization |
|
Describes the accuracy of NTP time. It can take values from 1 to 15 or as NA (not applicable) if NTP server is not reachable. |
File System Parameters
Parameter |
Description |
---|---|
|
Total amount of the IFE server disk size in kilobytes |
|
Total amount of used disk size on the IFE server disk in kilobytes |
|
Total amount of unused disk space on the IFE server disk in kilobytes |
|
Amount of corrupted disk space on the IFE server disk in kilobytes |
System Parameters
Parameter |
Description |
---|---|
|
Status of the CPU:
|
|
Status of the boot memory |
|
Status of EEPROM |
|
Status of the file system |
|
Status of PHY 1 hardware |
|
Status of PHY 2 hardware |
|
Status of the execution memory |
IFE Operating Time Parameters
Statistic |
Description |
---|---|
|
Operating time of IFE server |
Device Name Configuration Procedure
Step |
Action |
Result |
---|---|---|
1 |
From the IFE menu bar, click . |
Opens the page. |
2 |
From the menu, in the submenu, click . |
Opens the page. |
List of Parameters in Device Identification
Parameter |
Description |
---|---|
|
Device name which is updated in the device name field |
|
Name of the product |
|
Device serial number |
|
Device model number |
|
Current firmware version |
|
Combination of MAC address and the time |
|
Unique MAC address |
|
IP address of the IFE server |
|
Address used to communicate on the local network |