XB5 Selector Switches

Refer to Catalog DIA5ED2121213EN

XB5 Selector Switches

ZB5AD•

Standard Lever

ZB5AJX•

Extended Lever

Non-Illuminated Selector Switches

Color

Number and Type of Positions

Standard Lever [1]

Extended Lever [1]

Catalog Number

Black

2-maintained

ZB5AD2

ZB5AJ2

Black

2-momentary from
right to left

ZB5AD4

ZB5AJ4

Black

3-maintained

ZB5AD3

ZB5AJ3

Black

3-momentary to center

ZB5AD5

ZB5AJ5

Black

3-momentary from
left to center

ZB5AD7

ZB5AJ7

Black

3-momentary from
right to center

ZB5AD8

ZB5AJ8

ZB5AG•

Non-Illuminated Key Switches

Type of Operator

Number and Type of Positions

Catalog Number [2]

Key (No. 455)
[2]


NOTE: The symbol indicates key withdrawal position(s).

2-maintained

ZB5AG2

ZB5AG4

ZB5AG02

2-momentary from
right to left

ZB5AG6

3-maintained

ZB5AG0

ZB5AG3

ZB5AG5

ZB5AG9

ZB5AG09

3-momentary from
left to center

ZB5AG1

3-momentary to center

ZB5AG7

3-momentary from right to center

ZB5AG8

ZB5AG08

ZB5AG05

Sequence of Contacts on Selector Switch Bodies

Unit Type

Selector Switches

2-position

3-position

Note:

L=Left, C=Center, R=Right,
O=Open, X=Closed

Operator Plunger Position

Up

 

Down

 

Contact Block Location

L

C

R

L

C

R

L

C

R

L

C

R

L

C

R

Contacts

N.O.

O

O

O

X

X

X

X

X

O

O

O

O

O

X

X

N.C.

X

X

X

O

O

O

O

O

X

X

X

X

X

O

O

Footnotes

  1. For colored lever, add the following code to the end of catalog number: 01—white, 03—green, 04—red, 05—yellow, 06—blue (Example: ZB5AD204).
  2. Other key numbers:
    —key no. 421E: add the suffix 12 to the catalog number.
    —key no. 458A: add the suffix 10 to the catalog number.
    —key no. 520E: add the suffix 14 to the catalog number.
    —key no. 3131A: add the suffix 20 to the catalog number.
    —key no. 8D1: add the suffix D to the catalog number.
    Example: The catalog number for a head with key no. 421E for a 2 position maintained, lockable selector switch, with key withdrawal from the left-hand position, becomes: ZB5AG212
Feedback