Production Environment Scenarios

Refer to Catalogs DIA5ED2121212EN*, DIA5ED2121213EN**, DIA5ED2120503EN***, and 9001CT1103****

Introduction

Schneider Electric provides various products for usage in setting up and automating production system environments. The illustrations below provide examples of how to use the Harmony and XB/XV series products in a production environment.

The following illustration serves as an example of a product application map, showing how Schneider Electric’s Harmony and XB/XV series components can be incorporated throughout an automated production line for:

  • Machine control

  • Safety

  • Signaling

  • Remote operation

  • Access management

It demonstrates where each component type typically fits within a industrial environment, and is a reference for designing modern automated production systems where reliability, safety, and intuitive interaction are critical.



See the links in the table below for more detail information on the components in the above image.



The image below is an industrial automation illustration that shows various Harmony series control and signaling devices integrated into a factory or production line environment. This example highlights how different components connect to and support the operation of an automated machinery setup.

The image shows how the components are connected visually to a factory assembly line, demonstrating how the Harmony devices support control, safety, communication, and visualization in industrial automation systems.



See the links in the table below for more detail information on the components in the above image.

Feedback